Sustainable | Customizable | Efficient
Service
Sustainable | Customizable | Efficient
No alt text found for image

Copenhagen Airport is energy renovating with 3D-printed lighting solution

Background

Copenhagen Airport (hereinafter CPH) has the ambition of becoming emission-free by 2050. This involves air traffic as well as operations, and it was therefore also with sustainability in mind that they in the Spring of 2020 had to renovate a number of offices in the airport’s terminal 3. When it comes to energy renovation, price and savings are in focus. It was therefore important for CPH that the solution should provide significant energy savings while having a short payback time

No alt text found for image

Solution

In collaboration with Signify CPH chose to replace 250 conventional downlights with the tailormade and 3D-printed GreenSpace Downlights with PerfectFit from Philips. The downlight is printed from recycled polycarbonate, which reduces CO2 emissions by 76%. At the same time, the lighting technology in the downlight consists of an LED board, which significantly reduces energy consumption compared to similar, conventional downlights. In an office like this, with need for light 24 hours a day, this is of great importance. PIR sensors were installed in the toilets for extra savings when no presence was detected.

Especially when renovating recessed lighting solutions, it is a challenge to find luminaires that fits the cut out 1:1. With Philips’ PerfectFit solution, however, it was possible for CPH to get a tailormade solution that would fit directly into the existing cut outs. Thus, it was not necessary to replace the ceiling, which kept the project budget down. The mounting of the 250 downlights was made by the installer Kemp & Lauritzen. Kemp & Lauritzen’s electricity chairman at the airport, Henrik Nielsen, points out how the installation was easy and straightforward, due to the matching cut outs.

The result

CPH wanted an energy-efficient and sustainable lighting solution in the energy renovation of their offices in Terminal 3. By replacing the conventional downlights with an energy consumption of 39.6W per piece, with the sustainable LED downlights with an energy consumption of 12.5W, they have reduced the total energy consumption of the office by 68%. This corresponds to 60,000 kWh per year. At the same time, the 3D-printed solution meant that the budget for the project could be kept to a minimum, as the 3D-printed downlights could be mounted directly in the existing installation

No alt text found for image
No alt text found for image

Sustainable solution

With 3D print technology, GreenSpace Downlight is designed for the circular economy. The downlight is printed with recycled polycarbonate that can be recycled over and over again to further CO2 reductions.

No alt text found for image

Great energy savings

In an office with activity around the clock, the conversion to LED is noticeable. By switching from conventional downlights to LED, Copenhagen Airport saves 60,000 kWh annually

No alt text found for image

Easy installation with PerfectFit

The 3D-printed downlights are easy to mount in the existing installation, as they with PerfectFit are specially designed for the specific cut-out